Sidewall Bearing Pressure

The cable sidewall bearing pressure is the radial pressure experienced by the cable as it is pulled through a curved secdon. The parameters which influence SWBP are tension and radius of curvature of the bend. The pressure calculated by the equations in the table below must not exceed 500 Ib/ft. The equation variables are:

  • SWBP = Sidewall bearing pressure (lb/ft)
  • T = Tension exiting the bend (lb)
  • Ri = Inside bending radius (ft)
  • Wc = Weight correction factor (dimensionless)

Sidewall Bearing Pressure Equations

Configuration of Cables

Equation

Single

Triangular

Cradled

Diamond

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?