Fiber Manager Data Model Overview

This data model description is intended to assist anyone who is implementing Schneider Electric's Fiber Manager application. This document provides information about the features, objects, fields and relationships used in the data model. In addition to basic descriptions, there are also suggestions for when a field can be safely deleted from the model. This section also identifies all of the fields required for the application. An organization can always choose to hide a required field (but not delete it!), using the ArcFM Properties Manager.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?