Customer Connection

CustomerConnection contains information about the service provided to the customer.

Associations: ServiceAddress

Subtypes: None

Model Names: None

Attributes:

Field Name

Field Type

Description

Address

text

Customer address.

Alternate[X,Y,Z]

double

Stores the X, Y, and Z values from a GPS device.

AlternateSource

text

This field contains a value from the Feature Source domain that indicates an alternate source for the structure.

ConnectionType

text

Type of connection.

PhaseDesignation

long integer

Code indicating phases present; domain values include A, AB, AC, etc. Feeder Manager requires the PHASEDESIGNATION model name on this field for both ServicePoints and PrimaryMeters.

ServiceCurrentRating

short integer

Code indicating maximum rating of service delivered to CustomerConnection; domain values include 100 amps, 600 amps, etc.

International Data Model

In addition to the attributes listed above, the following attribute is used by the international electric data model.

Field Name

Description

CIS_ID

ID of customer as known to a Customer Information System (CIS).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?