Secondary Circuit Analysis Tables
Secondary Circuit Analysis is an electrical calculation (available in Designer) to easily perform "what-if" scenarios and determine which type of equipment will maximize the network's performance and minimize costs. Below are descriptions of the tables and fields required for Secondary Circuit Analysis. These tables must be owned by SDE.
MMENG_CONDUCTOR_ELEC
Field |
Data Type |
Description |
Units |
How Used |
---|---|---|---|---|
ID |
long integer |
A unique ID identifying the row in the table. |
|
|
Code |
text |
A unique value for GIS features. |
|
Serves as a lookup key when mapping GIS features onto rows in this table. |
CUCode |
text |
Not currently used. |
|
|
Description |
text |
A description of the conductor feature. |
|
|
R_Per1000_Units_Length |
double |
Positive sequence resistance per 1000 units length. |
|
|
X_Per1000_Units_Length |
double |
Positive sequence reactance per 1000 units length. |
|
|
Ampacity |
double |
Continuous current carrying capacity, in Amperes. |
|
|
R0_Per1000_Units_Length |
double |
Zero sequence resistance per 1000 units length. |
|
|
X0_Per1000_Units_Length |
double |
Zero sequence reactance per 1000 units length. |
|
|
Cost_PerUnitLength |
double |
Material cost per unit length of the conductor, in local currency. This value must be greater than 0. |
|
|
Material |
text |
Contains the conductor material (such as AL, CU, ACSR). |
|
|
Size_ |
text |
The diameter of the conductor. |
in. |
|
Underground |
short integer |
A yes/no value indicating whether the conductor is underground or overhead. Yes=Underground, No=Overhead. |
|
|
Insulation |
text |
Contains the type of insulation used by the conductor. The presence or absence of a non-blank insulation type is taken to imply an underground (non-blank value) or an overhead (blank value) conductor. Typical values (besides a blank value): XLP, Poly. |
|
Used to determine the inter-conductor spacing that is assumed. |
MMENG_CONDUCTOR_ELEC_ORIG
This table is for internal use only.
MMENG_TRANSFORMER
Field |
Data Type |
Description |
Units |
How Used |
---|---|---|---|---|
ID |
long integer |
A unique ID identifying the row in the table. |
|
|
Code |
text |
A unique ID for GIS features. |
|
Serves as a lookup key when mapping GIS features onto rows in this table. |
CUCode |
text |
Not currently used. |
|
|
Percent_Z_Min |
double |
Minimum impedance, as percent of rated kVA |
|
|
Percent_Z_Max |
double |
Maximum impedance, as percent of rated kVA |
|
|
Percent_X_Min |
double |
Not currently used by Secondary Circuit Analysis. |
|
|
Percent_X_Max |
double |
Not currently used by Secondary Circuit Analysis. |
|
|
Percent_R_Min |
double |
Not currently used by Secondary Circuit Analysis. |
|
|
Percent_R_Max |
double |
Not currently used by Secondary Circuit Analysis. |
|
|
NoLoad_Loss_Min |
long integer |
Not currently used by Secondary Circuit Analysis. |
|
|
NoLoad_Loss_Max |
long integer |
Not currently used by Secondary Circuit Analysis. |
|
|
Full_Load_Loss_Min |
long integer |
Not currently used by Secondary Circuit Analysis. |
|
|
Full_Load_Loss_Max |
long integer |
Not currently used by Secondary Circuit Analysis. |
|
|
EX_Min |
double |
Not currently used by Secondary Circuit Analysis. |
|
|
EX_Max |
double |
Not currently used by Secondary Circuit Analysis. |
|
|
X_to_R_Min |
double |
Ratio of reactance to resistance, for the maximum impedance value. |
|
|
X_to_R_Max |
double |
Ratio of reactance to resistance, for the minimum impedance value. |
|
|
Description |
text |
A description of the transformer feature. |
|
|
Phasing |
text |
The number of phases on the transformer (1 or 3). |
|
This value determines whether the secondary circuit will be modeled as a single-phase circuit with neutral return, or as a balanced 3-phase circuit. |
kVA |
double |
The nameplate kVA rating of the transformer. |
|
|
Type_ |
text |
Indicates the type of transformer. Typical values: pole, pad, pad mounted, pad mounted network, pole stepdown, deadfront pad mounted. |
|
|
High_Side_Voltage |
text |
The amount of voltage coming into the transformer. |
|
|
Low_Side_Voltage |
text |
The amount of voltage leaving the transformer. |
|
|
Cost |
double |
Material cost of the transformer, in local currency. |
local currency |
|
Min_R_Per1000_Units_Length |
double |
Positive sequence resistance per 1000 units length. Used for calculations that wish to err on the side of underestimating conductor impedance. |
|
Used by Design Optimization for fault calculations. |
Min_X_Per1000_Units_Length |
double |
Positive sequence reactance per 1000 units length. Used for calculations that wish to err on the side of underestimating conductor impedance. |
|
Used by Design Optimization for fault calculations. |
MMENG_ TRANSFORMER_ORIG
This table is for internal use only.