Load Summary

Demand from the customer is the load at receiving terminals averaged over a specific time. Demand is expressed in real power, apparent power, or current—kilowatts, reactive volt-amperes, volt-amperes, or amperes.

Associations: None

Subtypes: None

Model Names: LOADSUMMARY

Attributes:

Field Name

Field Type

Description

CurrentTotal

long integer

Amount of current in LoadSummary.

kVAR

long integer

Reactance in reactive volt-amperes.

kW

long integer

Load summary in kW.

Voltage

long integer

Voltage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?