GasPressureSystem
The gas pressure system is a continuous flow system with common Maximum Allowable Operating Pressure (MAOP) and System Operating Pressure (SOP) bound by the Town Border Station, Regulator Station, dead end, or a normally closed valve.
Subtypes: None
Associations: GasSystem, EmergencyIsolationsSystem
Model Names: None
Attributes:
Field Name |
Field Type |
Description |
---|---|---|
Comments |
text |
User and designer comments. |
GasSystemObjectID |
long integer |
ObjectID of associated GasSystem. |
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
MAOPEntered |
double |
Maximum Allowable Operating Pressure, in any unit of measure. |
MAOPStandard |
double |
Derived field displaying calculated standard Maximum Allowable Operating Pressure. |
MAOPUnitOfMeasure |
text |
MAOP standard unit of measure; examples include psi, iwc, etc. |
SOPEntered |
double |
System Operating Pressure, in any unit of measure. |
SOPRange |
text |
Range of System Operating Pressure. |
SOPStandard |
double |
Derived field displaying calculated standard System Operating Pressure. |
SOPUnitOfMeasure |
text |
Standard unit of measure for System Operating Pressure. |