Add Attribute Fields to Relationship Tables

After you create a new relationship, the “Relationship class is attributed” option lets you add the required NetworkID attribute field.

To add an attribute field:

  1. In the Catalog pane, expand your database until you find your newly created relationships.

  2. Right-click the relationship and choose Add to Current Map (or Add to New Map if you do not have a map open yet). This step moves the relationship into the Contents pane, where you can open it.

  3. In the Contents pane, right-click the relationship and choose Open.

  4. In the table view, next to Field, click the Add button.

  5. Add the following attribute field:

    • NetworkID (text with 255 characters)

  6. At the top of the application, on the Fields menu > Changes tool group, click Save.

  7. Repeat with all newly added relationships.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.