Relationships

DHFC leverages GIS relationships to maintain data integrity, inform tracing, perform queries, and other functions. It is a beneficial way to relate feature classes with a physical presence on the map with object tables that do not. For example, an RFCoupler is a point feature class with a geographic location, and it has multiple RFCoupler Ports that are records in an object table. These two have a relationship so the application knows which ports belong to which coupler, and there are subsequent relationships to track what is connected to each port.

  • Similar to the feature classes and object tables, relationships also follow the design and as-built geodatabase architecture, and there is a relationship for both states. For example, there is an RFCoupler_RFCouplerPort relationship, and an RFCoupler_RFCouplerPort_D relationship.

  • The name of the relationship itself is not referenced by the application and is at your discretion. However, for ease and consistency, Schneider Electric recommends a naming convention of origin_destination, as seen in RFCoupler_RFCouplerPort, for all relationships.

  • The relationship can be located in the root geodatabase, or it can be located within a dataset as long as either the origin or destination resides in the same dataset.

  • Every relationship has an equivalent tag in the schema.xml. See the topic <Relationship> and <ManyRelationship> Tags for more information.

  • Attributed relationships create a separate table to store attributes. Refer to the Add Attribute Fields to Relationship Tables topic for more information.

  • Refer to Esri’s Create Relationship Class article for steps to create relationships in ArcGIS Pro.

IMPORTANT: The Forward and Backward label names used by the relationships are referenced in the schema.xml. In other words, they must match the schema.xml for the application to function. The label names are different than the relationship class name.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.