RFPadData

DHFC object name: RFPadData

GIS design table name: RFPad_D

GIS built table name: RFPad

GIS table type: ObjectClass

Geometry type: Any


Fields

Name

Alias

Type

Domain

Length

Precision

Nullable

Field Role

Data Transfer

CatalogId

CatalogId

Guid

FALSE

Required

BiDirectional

EsriId

OBJECTID

ObjectId

FALSE

Required

BiDirectional

ModelNumber

Model Number

String

50

TRUE

Required

BiDirectional

NetworkId

NetworkId

String

200

FALSE

Required

BiDirectional

Workflow_Status

Workflow Status

String

WorkflowState

FALSE

Required

BiDirectional

CreationUser

Creation User

String

50

TRUE

Optional

BiDirectional

DateCreated

Date Created

Date

TRUE

Optional

BiDirectional

DateModified

Date Modified

Date

TRUE

Optional

BiDirectional

Direction

Direction

SmallInteger

ForwardReturnDomain

TRUE

Optional

ToGisOnly

InventoryNum

Inventory Number

String

50

TRUE

Optional

ToGisOnly

LastUser

Last User

String

50

TRUE

Optional

BiDirectional

Manufacturer

Manufacturer

String

50

TRUE

Optional

ToGisOnly

Value

Pad Value

String

50

TRUE

Optional

ToGisOnly


Required Fields

Field Name

Notes

NetworkID

Unique identifier for the component or record.

ObjectID

Esri Object ID for the feature or object.

GlobalID

Esri Global ID for the feature or object.

CatalogId

The Id of the DHFC catalog spec associated with the component; should be a string representation of a valid GUID in the following format, 6A1F97AD-C665-4521-B954-29A4429FC128.

ModelNumber

The component model number.

Workflow_Status

WorkflowState enumeration: AsBuilt and Proposed


Relationships

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.