RFPowerInserter_RFPowerInserterPort

There are two versions of this relationship:

  • RFPowerInserter_RFPowerInserterPort for the as-built representation.

  • RFPowerInserter_RFPowerInserterPort_D for the design representation.

RFPowerInserter_RFPowerInserterPort, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

RFPowerInserter_RFPowerInserterPort

Origin Table or Feature Class

RFPowerInserter

Destination Table or Feature Class

RFPowerInserterPort

Relationship Type

Simple

Forward Label

RFPowerInserterPort

IMPORTANT: The Forward Label you type while creating the relationship must match the EsriBuiltName entry in the schema.xml file for this component.

Backward Label

RFPowerInserter

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Relationship Attributes

No, I do not want to add attributes to this relationship class.

Primary Key

NetworkId

Foreign Key

PowerInserterId

RFPowerInserter_RFPowerInserterPort _D, the Design Relationship

Relationship Class Property

Value or Choice

Name

RFPowerInserter_RFPowerInserterPort_D

Origin Table or Feature Class

RFPowerInserter_D

Destination Table or Feature Class

RFPowerInserterPort_D

Relationship Type

Simple

Forward Label

SECom.ARCFM.RFPowerInserterPort

IMPORTANT: The Forward Label you type while creating the relationship must match the EsriDesignName entry in the schema.xml file for this component.

Backward Label

SECom.ARCFM.RFPowerInserter

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Relationship Attributes

No, I do not want to add attributes to this relationship class.

Primary Key

NetworkId

Foreign Key

PowerInserterId

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.