Conditioning Tap Properties

Point Size (required)

Assign a point value to a component based on physical size. With a consistent point value system you will be able to determine how much equipment can fit inside an enclosure. For example, if you have a pedestal rated to hold 30 points worth of components, then you can situate three 2-port taps rated at 10 points each into the box. A fourth 2-port tap would total 40 points, exceeding the rated 30 points of the pedestal.

Port Count (required)

The number of ports.

Tap Value (required)

The forward loss, in decibels, that the signal will drop on the tap leg.

Maximum Amperage

The amps that the manufacturer rates as maximum for the node.

Self Terminating (default: not selected)

Select the checkbox to mark the tap as self-terminating.

Through Leg

  • Forward Loss (required): The amount of forward signal loss at a particular frequency.

  • Return Loss (required): The amount of return signal loss at a particular frequency.

Tap Leg

  • Forward Loss (required): The amount of forward signal loss at a particular frequency.

  • Return Loss (required): The amount of return signal loss at a particular frequency.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.