RFNode_RFSegmentableNodeBoundary

There are two versions of this attributed relationship:

  • RFNode_RFSegmentableNodeBoundary for the as-built representation.

  • RFNode_RFSegmentableNodeBoundary_D for the design representation.

RFNode_RFSegmentableNodeBoundary, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

RFNode_RFSegmentableNodeBoundary

Origin Table or Feature Class

RFNode

Destination Table or Feature Class

RFSegmentableNodeBoundary

Relationship Type

Simple

Forward Label

RFSegmentableNodeBoundary

Backward Label

RFNode

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Attributed

Check the box for “Relationship class is attributed.” After the relationship is created, you then add attribute fields to the table. Refer to the Add Attribute Fields to Relationship Tables for more information.

Origin Primary Key

NetworkId

Origin Foreign Key

NodeNetworkId

Destination Primary Key

NetworkId

Destination Foreign Key

SegmentableBoundaryNetworkId

RFNode_RFSegmentableNodeBoundary_D, the Design Relationship

Relationship Class Property

Value or Choice

Name

RFNode_RFSegmentableNodeBoundary_D

Origin Table or Feature Class

RFNode_D

Destination Table or Feature Class

RFSegmentableNodeBoundary_D

Relationship Type

Simple

Forward Label

RFSegmentableNodeBoundary_D

Backward Label

RFNode_D

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Attributed

Check the box for “Relationship class is attributed.” After the relationship is created, you then add attribute fields to the table. Refer to the Add Attribute Fields to Relationship Tables for more information.

Origin Primary Key

NetworkId

Origin Foreign Key

NodeNetworkId

Destination Primary Key

NetworkId

Destination Foreign Key

SegmentableBoundaryNetworkId

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.