RFCable_OverheadSpan

There are two versions of this attributed relationship:

  • RFCable_OverheadSpan for the as-built representation.

  • RFCable_OverheadSpan_D for the design representation.

RFCable_OverheadSpan, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

RFCable_OverheadSpan

Origin Table or Feature Class

RFCable

Destination Table or Feature Class

OverheadSpan

Relationship Type

Simple

Forward Label

OverheadSpan

Backward Label

RFCable

Message Direction

None (no messages propagated)

Cardinality

M-N (many to many)

Attributed

Check the box for “Relationship class is attributed.” After the relationship is created, you then add attribute fields to the table. Refer to the Add Attribute Fields to Relationship Tables for more information.

Origin Primary Key

NetworkId

Origin Foreign Key

RFCableNetworkId

Destination Primary Key

NetworkId

Destination Foreign Key

OverheadSpanNetworkId

RFCable_OverheadSpan_D, the Design Relationship

Relationship Class Property

Value or Choice

Name

RFCable_OverheadSpan_D

Origin Table or Feature Class

RFCable_D

Destination Table or Feature Class

OverheadSpan

Relationship Type

Simple

Forward Label

OverheadSpan

Backward Label

RFCable_D

Message Direction

None (no messages propagated)

Cardinality

M-N (many to many)

Attributed

Check the box for “Relationship class is attributed.” After the relationship is created, you then add attribute fields to the table. Refer to the Add Attribute Fields to Relationship Tables for more information.

Origin Primary Key

NetworkId

Origin Foreign Key

RFCableNetworkId

Destination Primary Key

NetworkId

Destination Foreign Key

OverheadSpanNetworkId

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.