Taps Through Leg

Remove: Click the Remove button to the right of the value that you want to delete.

Add: Type the appropriate value(s) and click the Add button to the right of the value(s) you are adding.

Edit an existing value: Double-click the existing value and type a new value, then click Update to save all changes.

  • Forward Through Loss (required): The amount of forward through signal loss at particular frequencies.

  • Return Through Loss (required): The amount of return through signal loss at particular frequencies.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.