RFNodeCoaxPortData

DHFC object name: RFNodeCoaxPortData

GIS design table name: RFNodeCoaxPort_D

GIS built table name: RFNodeCoaxPort

GIS table type: ObjectClass

Geometry type: Any


Fields

Name

Alias

Type

Domain

Length

Precision

Nullable

Field Role

Data Transfer

ConnectedItemId

ConnectedItemId

Guid

FALSE

Required

BiDirectional

EsriId

OBJECTID

ObjectId

FALSE

Required

BiDirectional

IsPowerOnly

Is Power Only

SmallInteger

EsriYesNoEnum

FALSE

Required

BiDirectional

NetworkId

NetworkId

String

200

FALSE

Required

BiDirectional

NodeId

NodeId

Guid

FALSE

Required

BiDirectional

PortNumber

Port Number

SmallInteger

FALSE

Required

BiDirectional

Workflow_Status

Workflow Status

String

WorkflowState

FALSE

Required

BiDirectional

CreationUser

Creation User

String

50

TRUE

Optional

BiDirectional

DateCreated

Date Created

Date

TRUE

Optional

BiDirectional

DateModified

Date Modified

Date

TRUE

Optional

BiDirectional

HomesPassed

Homes Passed

Integer

TRUE

Optional

ToGisOnly

LastUser

Last User

String

50

TRUE

Optional

BiDirectional

PortName

Port Name

String

5

TRUE

Optional

ToGisOnly


Required Fields

Field Name

Notes

NetworkID

Unique identifier for the component or record.

ObjectID

Esri Object ID for the feature or object.

GlobalID

Esri Global ID for the feature or object.

ConnectItemId

The Network ID of the component that is connected downstream to the amplifier on the specified port.

NodeId

The Network ID of the node to which this port data corresponds.

PortNumber

The port number on the component to which the connection data applies.

Workflow_Status

WorkflowState enumeration: AsBuilt and Proposed


Relationships

None.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.