General

The General tab provides configurations that affect functionality in the DHFC client application. These settings include:

  • Set component layout offsets.

  • Ability to enable booster amps in a cascade.

    NOTE: Mixed signal oscilloscopes do not count the booster amplifier in the active cascade count.
  • Select which components generate tombstones.

  • Select the unit of measure, either Standard (US) or Metric.

  • Configure the cable length calculation factors to account for additional cable length in aerial or underground risers.

  • Set the default address search country to increase performance and reduce irrelevant hits when using the Address Search Tab.

Always click Save after making any changes. Changes are seen in the DHFC client application the next time a user logs in.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.