GIS Symbology

Some of the upcoming components have a field called GIS Symbology.

GIS Symbology provides you with the ability to specify symbology text for various component specifications in Catalog. This text is published to GIS with DHFC features and can be used as a basis for symbology.

Components that have this SpecSymbology field are:

  • Amplifiers

  • Cables

  • Connectors

  • Directional Couplers

  • Inline Equalizers

  • Nodes

  • Power Inserters

  • Power Supplies

  • Splices

  • Tap

  • Terminators

  • Underground Structure

The field must be added to the feature classes (listed above) in your GIS database:

  • Field Name: SpecSymbology

  • Data Type: Text

  • Max Length: 50 characters

Changes to the SpecSymbology field in GIS are ignored. The DHFC application does not use this text in any way.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.