Application Settings

Application Settings are high-level configurations that affect the DHFC client application. Here, you can configure:

  • Offset distance for components placed during auto-layout.

  • Which components are included in tombstone printing.

  • Unit of measure.

  • Additional cable lengths to account for aerial or underground risers.

  • Underground structures.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.