Schema

The schema.xml file provides a mapping between the ArcGIS feature service and the DHFC application objects. Refer to the Schema.xml Configuration File topic for more information about the file itself. The Solution Center Schema tab is used for uploading the file once it is complete.

On the Schema tab, you can download the current schema file and upload the schema file after editing it.

IMPORTANT: The schema file must be a properly formatted XML file in the structure outlined in the Schema.xml Configuration File topic. Schema changes are immediately available to the DHFC client application. Always back up your current file prior to uploading a new one. Uploading a file overwrites the entire contents of the current schema file.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.