RFPad_RFAmplifier_Fwd

There are two versions of this relationship:

  • RFPad_RFAmplifier_Fwd for the as-built representation.

  • RFPad_RFAmplifier_Fwd_D for the in-design representation.

RFPad_RFAmplifier_Fwd, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

RFPad_RFAmplifier_Fwd

Origin Table or Feature Class

RFPad

Destination Table or Feature Class

RFAmplifier

Relationship Type

Simple

Forward Label

RFAmplifier

Backward Label

RFPad

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Relationship Attributes

No, I do not want to add attributes to this relationship class.

Primary Key

NetworkId

Foreign Key

ForwardPadId

RFPad_RFAmplifier_Fwd_D, the Design Relationship

Relationship Class Property

Value or Choice

Name

RFPad_RFAmplifier_Fwd_D

Origin Table or Feature Class

RFPad_D

Destination Table or Feature Class

RFAmplifier_D

Relationship Type

Simple

Forward Label

SECom.ARCFM.RFAmplifier

Backward Label

SECom.ARCFM.RFPad

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Relationship Attributes

No, I do not want to add attributes to this relationship class.

Primary Key

NetworkId

Foreign Key

ForwardPadId

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.