RFNodeData

The following table describes the attribute editing configuration options for each field, separated into these categories:

  • Can the Editable setting be changed?

    • This column answers the question, “Am I allowed to add or remove this field from Attribute Editor?” The default for the Editable tag is Editable=“false.” If the table below states “Yes,” then you are allowed to add the tag Editable=“true” to that field, if desired. It then appears in Attribute Editor in the application. Editable fields are inherently Viewable, even if the Viewable setting is not included in the schema.xml.

  • Can the Viewable setting be changed?

    • This column answers the question, “Am I allowed to add or remove this field from being viewed in Attribute Editor?” To do so, add the tag Viewable=“true.” Viewable fields do not have to be Editable. In other words, you can provide them to your users in a read-only mode. A “No” in the table below means the value from that field is presented to the user in another, more meaningful way than the raw data contained in the field, and you cannot change its viewable setting.

  • Are attributes imported from GIS?

    • A “Yes” in the table below means the data originate from the GIS. These fields should have a tag of Import=“true”, and that tag should not be changed in the schema.xml.

    • A “No” in the table below means the field is populated while working in the application.

  • Data Type

    • Because the default data type is “string,” notice that most of the entries in the table below state “Not Required.” This is because if you do not add a DataType tag, it uses the default string type.

  • Validation Options

    • Validation Options only apply to Editable fields. Because most of the fields are managed by the application, notice that most options in the table below state “None.”

  • Coded Domain Name

    • This lists the domain provided in the default schema.xml.

  • Notes

    • This column includes other information for that field.

Field Name (CoaxName)

Can Editable setting be changed?

Can Viewable setting be changed?

Are attributes imported from GIS?

Data Type

Validation Options

Coded Domain Name

Notes

EsriId

No

Yes

Yes

Not Required

None

   

NetworkId

No

Yes

Yes

Not Required

None

   

AerialStructureId

No

Yes

Yes

Not Required

None

   

Amperage

No

No

No

Not Required

None

   

CatalogId

No

Yes

Yes

Not Required

None

   

CoaxPortCount

No

Yes

No

Not Required

None

   

CreationUser

No

Yes

Yes

Not Required

None

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

DateCreated

No

Yes

Yes

Not Required

None

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

DateModified

No

Yes

Yes

Not Required

None

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

DesignFrequency

No

Yes

No

Not Required

None

 

This value comes from the active project file.

FedFromComponentId

No

Yes

Yes

Not Required

None

   

FiberPortCount

No

Yes

No

Not Required

None

   

Flipped

No

Yes

No

Not Required

None

   

ForwardOutputHighSignalLevel

No

No

No

Not Required

None

   

ForwardOutputLowSignalLevel

No

No

No

Not Required

None

   

InternalPowerMapping

No

No

Yes

Not Required

None

   

InventoryNum

No

Yes

No

Not Required

None

   

IsInMdu

No

Yes

Yes

Not Required

None

   

IsLocked

No

Yes

Yes

Not Required

None

 

The lock button on the device pane toggles the state of this property.

LastUser

No

Yes

Yes

Not Required

None

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

Manufacturer

No

Yes

No

Not Required

None

   

Market

No

Yes

No

Not Required

None

 

This value comes from the active project file.

ModelNumber

No

Yes

No

Not Required

None

   

Name

Yes

Yes

Yes

Not Required

MaxLength

 

This field does not appear in the Attribute Editor, but is editable at the top of the device pane. 

PortConfiguration

No

No

Yes

Not Required

None

 

See the topic RFNode and the PortConfiguration Field for more information.

PoweringFedFromComponentId

No

Yes

Yes

Not Required

None

   

PowerSupplyId

No

Yes

No

Not Required

None

   

ProjectFileCatalogId

No

Yes

Yes

Not Required

None

 
IMPORTANT: If the application encounters a null ProjectFileCatalogId (for example, if opening an older design prior to upgrading to 11.4 and beyond), the application falls back to locating the project file by name. This means, if both the ProjectFileCatalogId is null and the project file name has been changed, the older design cannot be loaded. Thus, during your transition to version 11.4 and beyond, do not change any project file names until after older designs are pushed or otherwise cleared from the system.

ProjectFileName

No

Yes

Yes

Not Required

None

   

ReturnInputHighSignalLevel

No

No

No

Not Required

None

   

ReturnInputLowSignalLevel

No

No

No

Not Required

None

   

SegmentationConfiguration

No

No

Yes

Not Required

None

 

This field is required if your company uses segmentable nodes. Otherwise, it is optional.

When a node is segmented, the SegmentationConfiguration field contains information about the nodes and the legs they serve. The length of this field should be the Node Name field length + 50. For example, if your Node Name field length is limited to 45, then this field’s length should be 95 (45 + 50).

When a node is not segmented, this field is null.

SegmentationMode

No

No

Yes

Not Required

None

NodeSegmentation

This field is required if your company uses segmentable nodes. Otherwise, it is optional.

SpecSymbology

No

Yes

No

Not Required

None

   

SymbolRotation

Yes

Yes

Yes

double

Range

   

TotalHomesPassed

No

No

No

Not Required

None

   

TotalHomesPassedLegA

No

No

No

Not Required

None

   

TotalHomesPassedLegB

No

No

No

Not Required

None

   

TotalHomesPassedLegC

No

No

No

Not Required

None

   

TotalHomesPassedLegD

No

No

No

Not Required

None

   

UGStructureId

No

Yes

Yes

Not Required

None

   

Voltage

No

No

No

Not Required

None

   

Workflow_Status

Yes

Yes

Yes

Not Required

None

WorkflowState

Can use FriendlyName="Workflow Status"

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.