RFEqualizer_RFAmplifier_Fwd

There are two versions of this relationship:

  • RFEqualizer_RFAmplifier_Fwd for the as-built representation.

  • RFEqualizer_RFAmplifier_Fwd_D for the design representation.

RFEqualizer_RFAmplifier_Fwd, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

RFEqualizer_RFAmplifier_Fwd

Origin Table or Feature Class

RFEqualizer

Destination Table or Feature Class

RFAmplifier

Relationship Type

Simple

Forward Label

RFAmplifier

Backward Label

RFEqualizer

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Relationship Attributes

No, I do not want to add attributes to this relationship class.

Primary Key

NetworkId

Foreign Key

ForwardEqId

RFEqualizer_RFAmplifier_Fwd_D, the Design Relationship

Relationship Class Property

Value or Choice

Name

RFEqualizer_RFAmplifier_Fwd_D

Origin Table or Feature Class

RFEqualizer_D

Destination Table or Feature Class

RFAmplifier_D

Relationship Type

Simple

Forward Label

SECom.ARCFM.RFAmplifier

Backward Label

SECom.ARCFM.RFEqualizer

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Relationship Attributes

No, I do not want to add attributes to this relationship class.

Primary Key

NetworkId

Foreign Key

ForwardEqId

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.