Solution Center Configuration for DHFC

Configuring your equipment catalogue early in the process is essential for a successful implementation. Some of the configuration is completed in DHFC and the rest in Solution Center. To properly configure DHFC, you work with Solution Center in tandem with configuring the geodatabase.

Several elements of configuration performed in Solution Center include:

  • Manage the equipment catalog.

  • Connect the DHFC application to the published map service.

  • Build reference maps for end users.

  • Control tombstone printing.

  • Choose units of measure.

  • Upload the schema.xml.

  • Export the equipment catalogue to Excel.

  • Import the equipment catalogue from Excel.

In Solution Center, select the DHFC plugin to get started.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.