Forward Loss and Return Loss

  • Remove: Click the Remove button to the right of the value that you want to delete.

  • Add: Type the appropriate value(s) and click the Add button to the right of the value(s) you are adding.

  • Edit an existing value: Double-click the existing value and type a new value, then click Update to save all changes.

    • Forward Loss: The amount of forward signal loss at particular frequencies.

    • Return Loss: The amount of return signal loss for at particular frequencies.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.