RFAmplifierPortData

DHFC object name: RFAmplifierPortData

GIS design table name: RFAmplifierPort_D

GIS built table name: RFAmplifierPort

GIS table type: ObjectClass

Geometry type: Any


Fields

Name

Alias

Type

Domain

Length

Precision

Nullable

Field Role

Data Transfer

AmplifierId

Amplifier Id

Guid

FALSE

Required

BiDirectional

ConnectedItemId

ConnectedItemId

Guid

FALSE

Required

BiDirectional

EsriId

OBJECTID

ObjectId

FALSE

Required

BiDirectional

NetworkId

NetworkId

String

200

FALSE

Required

BiDirectional

Workflow_Status

Workflow Status

String

WorkflowState

FALSE

Required

BiDirectional

CreationUser

Creation User

String

50

TRUE

Optional

BiDirectional

DateCreated

Date Created

Date

TRUE

Optional

BiDirectional

DateModified

Date Modified

Date

TRUE

Optional

BiDirectional

LastUser

Last User

String

50

TRUE

Optional

BiDirectional

PortNumber

Port Number

SmallInteger

TRUE

Optional

ToGisOnly


Required Fields

Field Name

Notes

NetworkID

Unique identifier for the component or record.

ObjectID

Esri Object ID for the feature or object.

GlobalID

Esri Object ID for the feature or object.

AmplifierId

The Network ID of the amplifier to which this port data corresponds.

ConnectedItemId

The Network ID of the component that is connected downstream to the amplifier on the specified port.

PortNumber

The port number on the component to which t the connection data applies.

Workflow_Status

WorkflowState enumeration: AsBuilt and Proposed.

Relationships

None.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.