Underground Structures Properties

Underground Structure Type (required)

Select the type from the drop-down.

TIP: Where does this drop-down come from? It comes from Solution Center > DHFC > Application Settings > Underground Structures.

Symbol Name

Type an abbreviation for the structure. This labels the structure in the map with the abbreviation. For example:

IMPORTANT: While the Symbol Name field accepts many characters, we strongly recommend to use abbreviations up to 2 characters. As you can see in the image above, 2 characters completely occupy the symbol, and any more would spill out onto the map.

Minimum Point Value (required) and Maximum Point Value (required)

The auto-optimization engine uses these values in calculations for optimizing your network design in Designer HFC.

  • The underground structure contains other components, and these values determine how many components and at what size can fit inside the cabinet.

    • While the underground structure has a range of values between a minimum and maximum, all other components have a single Point Size value.

  • For example, assume a cabinet has a Maximum Point Value of 210, a Node has a Point Size of 100, and an Amplifier has a Point Size of 50. That means one Node and two Amplifiers could fit inside that particular cabinet (100 + 50 + 50 = 200, which is less than 210). A cabinet that was rated at only 190 could not accommodate the same combination of components because it is too small.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.