RFPowerSupplyBoundary_RFPowerSupply

There are two versions of this attributed relationship:

  • RFPowerSupplyBoundary_RFPowerSupply for the as-built representation.

  • RFPowerSupplyBoundary_RFPowerSupply_D for the design representation.

RFPowerSupplyBoundary_RFPowerSupply, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

RFPowerSupplyBoundary_RFPowerSupply

Origin Table or Feature Class

RFPowerSupplyBoundary

Destination Table or Feature Class

RFPowerSupply

Relationship Type

Simple

Forward Label

RFPowerSupply

Backward Label

RFPowerSupplyBoundary

Message Direction

None (no messages propagated)

Cardinality

1–1 (one to one)

Attributed

Check the box for “Relationship class is attributed.” After the relationship is created, you then add attribute fields to the table. Refer to the Add Attribute Fields to Relationship Tables for more information.

Origin Primary Key

NetworkId

Origin Foreign Key

PowerSupplyBoundaryId

Destination Primary Key

NetworkId

Destination Foreign Key

PowerSupplyId

RFPowerSupplyBoundary_RFPowerSupply_D, the Design Relationship

Relationship Class Property

Value or Choice

Name

RFPowerSupplyBoundary_RFPowerSupply_D

Origin Table or Feature Class

RFPowerSupplyBoundary_D

Destination Table or Feature Class

RFPowerSupply_D

Relationship Type

Simple

Forward Label

RFPowerSupply

Backward Label

RFPowerSupplyBoundary

Message Direction

None (no messages propagated)

Cardinality

1–1 (one to one)

Attributed

Check the box for “Relationship class is attributed.” After the relationship is created, you then add attribute fields to the table. Refer to the Add Attribute Fields to Relationship Tables for more information.

Origin Primary Key

NetworkId

Origin Foreign Key

PowerSupplyBoundaryId

Destination Primary Key

NetworkId

Destination Foreign Key

PowerSupplyId

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.