RFAmplifier_RFAmplifierPort

There are two versions of this relationship:

  • RFAmplifier_RFAmplifierPort for the as-built representation.

  • RFAmplifier_RFAmplifierPort_D for the design representation.

RFAmplifier_RFAmplifierPort, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

RFAmplifier_RFAmplifierPort

Origin Table or Feature Class

RFAmplifier

Destination Table or Feature Class

RFAmplifierPort

Relationship Type

Simple

Forward Label

RFAmplifierPort

IMPORTANT: The Forward Label you type while creating the relationship must match the EsriBuiltName entry in the schema.xml file for this component.

Backward Label

RFAmplifier

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Relationship Attributes

No, I do not want to add attributes to this relationship class.

IMPORTANT: RFAmplifier_RFAmplifierPort does not require an attributed relationship.

Primary Key

NetworkId

Foreign Key

CouplerId

RFAmplifier_RFAmplifierPort_D, the Design Relationship

Relationship Class Property

Value or Choice

Name

RFAmplifier_RFAmplifierPort_D

Origin Table or Feature Class

RFAmplifier_D

Destination Table or Feature Class

RFAmplifierPort_D

Relationship Type

Simple

Forward Label

SECom.ARCFM.RFAmplifierPort_D

IMPORTANT: The Forward Label you type while creating the relationship must match the EsriDesignName entry in the schema.xml file for this component.

Backward Label

SECom.ARCFM.RFAmplifier_D

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Relationship Attributes

No, I do not want to add attributes to this relationship class.

Primary Key

NetworkId

Foreign Key

AmplifierId

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.