Power Supplies Properties

Point Size (required): Assign a point value to a component based on physical size. With a consistent point value system you will be able to determine how much equipment can fit inside an enclosure. For example, if you have a pedestal rated to hold 30 points worth of components, then you can situate three 2-port taps rated at 10 points each into the box. A fourth 2-port tap would total 40 points, exceeding the rated 30 points of the pedestal.

Voltage (required)

The amount of potential energy between two points on a circuit.

Amperage (required)

The amount of electrical charge (current) that flows through a conductor in a given time.

Maximum Load Percentage (required)

Maximum load in percentage.

Number of Batteries

The number of batteries that the power supply contains, if applicable.

Is Status Monitoring

A checkbox to denote that the power supply is performing status monitoring.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.