Project Validation

When you click the Validate Project File button, the application searches the project components and groupings, and flags those with attributes that violate the parameters set at the Project level.


If errors are found, the program creates a Validation Errors section that is grouped by component types having at least one item that violates the Project parameters.


Review Errors

If errors are present, click the expand button to view the errant component plus the specific errors associated with that component.


Copy Error Information

The Validation Errors section provides a clear summary of the component and error message. The Copy to Clipboard button provides the same information in addition to the GUID associated with the errant component.

  • At the Validation Errors level (the highest level), click the Copy to Clipboard button to copy all errors at the Project level.

  • To copy errors for a single component type, expand the component type first, then click the Copy to Clipboard button nested within that component’s error list.

NOTE: When an error applies to a specific component, the component’s GUID is listed within the error. When there is an issue with the configuration of the Grouping, the Grouping GUID is listed, since the Grouping is the source of the error rather than a component.


Error Codes

The error codes are comprised of 5 digits. The first 2 digits refer to the component type. For example, “02” refers to amplifiers. The last 3 digits refer to the error itself. The errors are specific to the component type and are not necessarily the same issue across all types. In other words, error “005” for amplifiers is a different issue than error “005” for directional couplers.

IMPORTANT: The leading “0” is dropped in the interface. Therefore, error “02005” appears as “2005” in the interface.


Component

Error Code

Description

Node, 01

01005

NodeFwdFrequenciesInvalid: The node has an invalid forward frequency profile.

01010

NodeRtnFrequenciesInvalid: The node has an invalid return frequency profile.

Amplifier, 02

02005

AmplifierFwdFrequencyProfileInvalidOnPort: The amplifier has an invalid forward frequency profile on a given port.

02010

AmplifierRtnInputFrequencyInvalid: The amplifier has an invalid return input frequency.

02015

AmplifierRtnOutputFrequencyInvalid: The amplifier has an invalid return output frequency.

02020

IncompatibleInternalEqForwardFrequencyProfile: The amplifier has an internal forward input equalizer with an incompatible frequency profile.

02025

IncompatibleInternalEqReturnFrequencyProfile: The amplifier has an internal return input equalizer with an incompatible frequency profile.

02030

AmplifierFwdFrequencyOutOfRange: The amplifier forward input frequency profile is outside of the acceptable range.

02035

AmplifierInternalComponentsMissing: No internal components could be found for the given amplifier.

02040

AmplifierInputInternalEqComponentsMissing: No input internal equalizer components could be found for the given amplifier.

02045

AmplifierOutputInternalEqComponentsMissing: No output internal equalizer components could be found for the given amplifier.

Amplifier Internal Equalizer, 04

04005

InternalAmpEqFwdFrequenciesInvalid: The forward internal amplifier equalizer frequencies are invalid.

04010

InternalAmpEqRtnFrequenciesInvalid: The return internal amplifier equalizer frequencies are invalid.

Tap, 05

05005

TapLegFrequenciesInvalid: The tap has an invalid forward frequency profile. Frequency profiles are merged and validated against the forward and return tracked frequencies of a project file.

05010

TapThroughLegFrequenciesInvalid: The tap has an invalid through leg frequency profile. Frequency profiles are merged and validated against the forward and return tracked frequencies of a project file.

Cable, 06

06050

InvalidCableFrequencyProfile: The cable has an invalid cable frequency profile.

06010

NoConnectorForCable: No pin connectors are in grouping that are compatible with the cable.

Splitter, 07

07050

SplitterFwdFrequencyProfileInvalidOnPort: The splitter has an invalid forward frequency profile on a given port.

07010

SplitterRtnFrequencyInvalidProfileOnPort: The splitter has an invalid return frequency profile on a given port.

Directional Coupler, 08

08050

DirectionalCouplerDownLegFrequenciesInvalid: The directional coupler has invalid forward or return down leg frequency profiles. Frequency profiles are merged and validated against the forward and return tracked frequencies of a project file.

08010

DirectionalCouplerThroughLegFrequenciesInvalid: The directional coupler has invalid forward or return through leg frequency profiles. Frequency profiles are merged and validated against the forward and return tracked frequencies of a project file.

Power Inserter, 09

09005

PowerInserterFrequenciesInvalid: The power inserter has invalid forward or return frequency profiles. Frequency profiles are merged and validated against the forward and return tracked frequencies of a project file.

Inline Equalizer, 12

12005

InlineEqualizerFrequenciesInvalid: The inline equalizer has invalid forward or return frequency profiles. Frequency profiles are merged and validated against the forward and return tracked frequencies of a project file.

Project File, 99

99005

NullProjectFile: The given project file resource was null.

99010

InvalidGrouping: The grouping on a project file is invalid.

99015

GroupingComponentsMissing: The grouping on a project file is invalid. It does not contain any components.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.