RFPowerInserterPortData

DHFC object name: RFPowerInserterPortData

GIS design table name: RFPowerInserterPort_D

GIS built table name: RFPowerInserterPort

GIS table type: ObjectClass

Geometry type: Any


Fields

Name

Alias

Type

Domain

Length

Precision

Nullable

Field Role

Data Transfer

ConnectedItemId

ConnectedItemId

Guid

FALSE

Required

BiDirectional

EsriId

OBJECTID

ObjectId

FALSE

Required

BiDirectional

NetworkId

NetworkId

String

200

FALSE

Required

BiDirectional

PortNumber

Port Number

SmallInteger

FALSE

Required

BiDirectional

PowerInserterId

PowerInserterId

Guid

FALSE

Required

BiDirectional

Workflow_Status

Workflow Status

String

WorkflowState

FALSE

Required

BiDirectional

CreationUser

Creation User

String

50

TRUE

Optional

BiDirectional

DateCreated

Date Created

Date

TRUE

Optional

BiDirectional

DateModified

Date Modified

Date

TRUE

Optional

BiDirectional

LastUser

Last User

String

50

TRUE

Optional

BiDirectional


Required Fields

Field Name

Notes

NetworkID

Unique identifier for the component or record.

ObjectID

Esri Object ID for the feature or object.

GlobalID

Esri Global ID for the feature or object.

ConnectedItemId

The Network ID of the component the power inserter is connected to on the given port.

PortNumber

The port number on the component to which the connection data applies.

PowerInserterId

The ID of the power inserter component.

Workflow_Status

WorkflowState enumeration: AsBuilt and Proposed


Relationships

None.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.