RFCable_Duct

There are two versions of this attributed relationship:

  • RFCable_Duct for the as-built representation.

  • RFCable_Duct_D for the design representation.


RFCable_Duct, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

RFCable_Duct

Origin Table or Feature Class

RFCable

Destination Table or Feature Class

Duct

Relationship Type

Simple

Forward Label

Duct

Backward Label

RFCable

Message Direction

None (no messages propagated)

Cardinality

M-N (many to many)

Attributed

Check the box for “Relationship class is attributed.” After the relationship is created, you then add attribute fields to the table. Refer to the Add Attribute Fields to Relationship Tables for more information.

Origin Primary Key

NetworkId

Origin Foreign Key

RFCableId

Destination Primary Key

NetworkId

Destination Foreign Key

DuctId

RFCable_Duct_D, the Design Relationship

Relationship Class Property

Value or Choice

Name

RFCable_Duct_D

Origin Table or Feature Class

RFCable_D

Destination Table or Feature Class

Duct

Relationship Type

Simple

Forward Label

Duct

Backward Label

RFCable_D

Message Direction

None (no messages propagated)

Cardinality

M-N (many to many)

Attributed

Check the box for “Relationship class is attributed.” After the relationship is created, you then add attribute fields to the table. Refer to the Add Attribute Fields to Relationship Tables for more information.

Origin Primary Key

NetworkId

Origin Foreign Key

RFCableId

Destination Primary Key

NetworkId

Destination Foreign Key

DuctId

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.