AddressPointData

The following table describes the attribute editing configuration options for each field, separated into these categories:

  • Can the Editable setting be changed?

    • This column answers the question, “Am I allowed to add or remove this field from Attribute Editor?” The default for the Editable tag is Editable=“false.” If the table below states “Yes,” then you are allowed to add the tag Editable=“true” to that field, if desired. It then appears in Attribute Editor in the application. Editable fields are inherently Viewable, even if the Viewable setting is not included in the schema.xml.

  • Can the Viewable setting be changed?

    • This column answers the question, “Am I allowed to add or remove this field from being viewed in Attribute Editor?” To do so, add the tag Viewable=“true.” Viewable fields do not have to be Editable. In other words, you can provide them to your users in a read-only mode. A “No” in the table below means the value from that field is presented to the user in another, more meaningful way than the raw data contained in the field, and you cannot change its viewable setting.

  • Are attributes imported from GIS?

    • A “Yes” in the table below means the data originate from the GIS. These fields should have a tag of Import=“true”, and that tag should not be changed in the schema.xml.

    • A “No” in the table below means the field is populated while working in the application.

  • Data Type

    • Because the default data type is “string,” notice that most of the entries in the table below state “Not Required.” This is because if you do not add a DataType tag, it uses the default string type.

  • Validation Options

    • Validation Options only apply to Editable fields. Because most of the fields are managed by the application, notice that most options in the table below state “None.”

  • Coded Domain Name

    • This lists the domain provided in the default schema.xml.

  • Notes

    • This column includes other information for that field.

Field Name (CoaxName)

Can Editable setting be changed?

Can Viewable setting be changed?

Are attributes imported from GIS?

Data Type

Validation Options

Coded Domain Name

Notes

EsriId

No

Yes

Yes

Not Required

None

   

NetworkId

No

Yes

Yes

Not Required

None

   

AerialStructureId

No

Yes

Yes

Not Required

None

 

Hidden on MDU Address points.

AmpId

No

Yes

No

Not Required

None

   

Cascade

No

Yes

No

Not Required

None

   

CommercialMDUCount

Yes

Yes

Yes

int/int32

Range

 

Hidden on regular address points.

CreationUser

No

Yes

Yes

Not Required

None

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

DateCreated

No

Yes

Yes

Not Required

None

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

DateModified

No

Yes

Yes

Not Required

None

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

HouseNo

Yes

Yes

Yes

Not Required

MaxLength

   

IsInMdu

No

Yes

Yes

Not Required

None

   

LastUser

No

Yes

Yes

Not Required

None

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

Market

No

Yes

No

Not Required

None

   

NetPath

No

Yes

No

Not Required

None

   

NodeId

No

Yes

No

Not Required

None

 

Can use FriendlyName="Node Id"

NodeLeg

No

Yes

No

Not Required

None

 

Can use FriendlyName="Node Leg"

PowerSupplyId

No

Yes

No

Not Required

None

 

Can use FriendlyName="Power Supply Id"

ResidentialMDUCount

Yes

Yes

Yes

int/int32

Range

 

Hidden on regular address points.

StreetName

Yes

Yes

Yes

Not Required

MaxLength

   

SymbolRotation

Yes

Yes

Yes

Not Required

None

 

Can use FriendlyName="Symbol Rotation"

TapId

No

Yes

Yes

Not Required

None

 

Can use FriendlyName="Tap Id"

TapId_D

No

Yes

Yes

Not Required

None

 

Can use FriendlyName="Tap Id_D"

UGStructureId

No

Yes

Yes

Not Required

None

 

Hidden on MDU Address points.

Workflow_Status

No

Yes

No

Not Required

None

 

Can use FriendlyName="Workflow Status"

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.