UndergroundSpan_Duct

There is no design representation of UndergroundSpan or Duct, therefore, only one version of this relationship is needed:

  • UndergroundSpan_Duct for the as-built representation.

UndergroundSpan_Duct, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

UndergroundSpan_Duct

Origin Table or Feature Class

UndergroundSpan

Destination Table or Feature Class

Duct

Relationship Type

Simple

Forward Label

Duct

IMPORTANT: The Forward Label you type while creating the relationship must match the EsriBuiltName entry in the schema.xml file for this component.

Backward Label

UndergroundSpan

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Relationship Attributes

No, I do not want to add attributes to this relationship class.

Primary Key

NetworkId

Foreign Key

UndergroundSpanId

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.