RFNode_RFNodeBoundary

There are two versions of this relationship:

  • RFNode_RFNodeBoundary for the as-built representation.

  • RFNode_RFNodeBoundary_D for the design representation.

RFNode_RFNodeBoundary, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

RFNode_RFNodeBoundary

Origin Table or Feature Class

RFNode

Destination Table or Feature Class

RFNodeBoundary

Relationship Type

Simple

Forward Label

RFNodeBoundary

IMPORTANT: The Forward Label you type while creating the relationship must match the EsriBuiltName entry in the schema.xml file for this component.

Backward Label

RFNode

Message Direction

None (no messages propagated)

Cardinality

1–1 (one to one)

Relationship Attributes

No, I do not want to add attributes to this relationship class.

Primary Key

NetworkId

Foreign Key

NodeNetworkId

RFNode_RFNodeBoundary_D, the Design Relationship

Relationship Class Property

Value or Choice

Name

RFNode_RFNodeBoundary_D

Origin Table or Feature Class

RFNode_D

Destination Table or Feature Class

RFNodeBoundary_D

Relationship Type

Simple

Forward Label

SECom.ARCFM.RFNodeBoundary

IMPORTANT: The Forward Label you type while creating the relationship must match the EsriDesignName entry in the schema.xml file for this component.

Backward Label

SECom.ARCFM.RFNode

Message Direction

None (no messages propagated)

Cardinality

1–1 (one to one)

Relationship Attributes

No, I do not want to add attributes to this relationship class

Primary Key

NetworkId

Foreign Key

NodeNetworkId

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.