High Tap Value Plugin Properties

Equalizer Value in dB (required)

The auto-optimization engine uses this value in calculations for optimizing your network design in Designer HFC.

Forward Loss (required): The amount of forward signal loss at a particular frequency.

Return Loss (required): The amount of return signal loss at a particular frequency.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.