Power Inserters Properties

Point Size (required): Assign a point value to a component based on physical size. With a consistent point value system you will be able to determine how much equipment can fit inside an enclosure. For example, if you have a pedestal rated to hold 30 points worth of components, then you can situate three 2-port taps rated at 10 points each into the box. A fourth 2-port tap would total 40 points, exceeding the rated 30 points of the pedestal.

Output Port Count (required)

The maximum number of output ports.

Power Inserter Loss

  • Remove: Click the Remove button to the right of the value that you want to delete.

  • Add: Type the appropriate value(s) and click the Add button to the right of the value(s) you are adding.

  • Edit an existing value: Double-click the existing value and type a new value, then click Update to save all changes.

    • Forward Loss (required): The amount of forward signal loss at particular frequencies.

    • Return Loss (required): The amount of return signal loss at particular frequencies.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.