RFCoupler_RFCouplerPort

There are two versions of this relationship:

  • RFCoupler_RFCouplerPort for the as-built representation.

  • RFCoupler_RFCouplerPort_D for the design representation.

RFCoupler_RFCouplerPort, the As-Built Relationship

Relationship Class Property

Value or Choice

Name

RFCoupler_RFCouplerPort

Origin Table or Feature Class

RFCoupler

Destination Table or Feature Class

RFCouplerPort

Relationship Type

Simple

Forward Label

RFCouplerPort

Backward Label

RFCoupler

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Relationship Attributes

No, I do not want to add attributes to this relationship class.

Primary Key

NetworkId

Foreign Key

CouplerId


RFCoupler_RFCouplerPort_D, the Design Relationship

Relationship Class Property

Value or Choice

Name

RFCoupler_RFCouplerPort_D

Origin Table or Feature Class

RFCoupler_D

Destination Table or Feature Class

RFCouplerPort_D

Relationship Type

Simple

Forward Label

SECom.ARCFM.RFCouplerPort

Backward Label

SECom.ARCFM.RFCoupler

Message Direction

None (no messages propagated)

Cardinality

1–M (one to many)

Relationship Attributes

No, I do not want to add attributes to this relationship class.

Primary Key

NetworkId

Foreign Key

CouplerId

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.