RFAmplifierData

The following table describes the attribute editing configuration options for each field, separated into these categories:

  • Can the Editable setting be changed?

    • This column answers the question, “Am I allowed to add or remove this field from Attribute Editor?” The default for the Editable tag is Editable=“false.” If the table below states “Yes,” then you are allowed to add the tag Editable=“true” to that field, if desired. It then appears in Attribute Editor in the application. Editable fields are inherently Viewable, even if the Viewable setting is not included in the schema.xml.

  • Can the Viewable setting be changed?

    • This column answers the question, “Am I allowed to add or remove this field from being viewed in Attribute Editor?” To do so, add the tag Viewable=“true.” Viewable fields do not have to be Editable. In other words, you can provide them to your users in a read-only mode. A “No” in the table below means the value from that field is presented to the user in another, more meaningful way than the raw data contained in the field, and you cannot change its viewable setting.

  • Are attributes imported from GIS?

    • A “Yes” in the table below means the data originate from the GIS. These fields should have a tag of Import=“true”, and that tag should not be changed in the schema.xml.

    • A “No” in the table below means the field is populated while working in the application.

  • Data Type

    • Because the default data type is “string,” notice that most of the entries in the table below state “Not Required.” This is because if you do not add a DataType tag, it uses the default string type.

  • Validation Options

    • Validation Options only apply to Editable fields. Because most of the fields are managed by the application, notice that most options in the table below state “None.”

  • Coded Domain Name

    • This lists the domain provided in the default schema.xml.

  • Notes

    • This column includes other information for that field.

Field Name (CoaxName)

Can Editable setting be changed?

Can Viewable setting be changed?

Are attributes imported from GIS?

Data Type

Validation Options

Coded Domain Name

Notes

EsriId

No

Yes

Yes

Not Required

None

   

NetworkId

No

Yes

Yes

Not Required

None

   

AerialStructureId

No

No

Yes

Not Required

None

   

Amperage

No

Yes

No

Not Required

None

   

AmpNumber

No

Yes

Yes

Not Required

None

 

Can use FriendlyName="Amp Number"

AmpType

Yes

Yes

No

CodedValueDomain

None

AmplifierType

Can use FriendlyName="Amp Type"

CascadeNumber

No

Yes

No

Not Required

None

 

Can use FriendlyName="Cascade Number"

CatalogId

No

Yes

Yes

Not Required

MaxLength

 

Can use FriendlyName="Catalog Id"

CreationUser

No

Yes

Yes

Not Required

MaxLength

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

DateCreated

No

Yes

Yes

Not Required

None

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

DateModified

No

Yes

Yes

Not Required

None

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

DistanceToLastActive

No

Yes

No

Not Required

None

 

Can use FriendlyName="Distance To Last Active (ft)"

FedFromComponentId

No

Yes

Yes

Not Required

None

   

Flipped

No

Yes

Yes

Not Required

None

   

ForwardInputHighLevel

No

Yes

No

Not Required

None

 

Can use FriendlyName="Fwd Input High (dBmV)"

ForwardInputLowLevel

No

Yes

No

Not Required

None

 

Can use FriendlyName="Fwd Input Low (dBmV)"

ForwardOutputHighLevel

No

Yes

No

Not Required

None

 

Can use FriendlyName="Fwd Output High (dBmV)"

ForwardOutputLowLevel

No

Yes

No

Not Required

None

 

Can use FriendlyName="Fwd Output Low (dBmV)"

GainControlMode

No

Yes

No

Not Required

None

 

Can use FriendlyName="Gain Control Mode"

HotDotPortNumber

No

Yes

Yes

Not Required

None

 

Can use FriendlyName="Hot Dot Port Number"

InternalCouplerCompanyID1

No

Yes

Yes

Not Required

MaxLength

   

InternalCouplerCompanyID2

No

Yes

Yes

Not Required

MaxLength

   

InternalCouplerCompanyID3

No

Yes

Yes

Not Required

MaxLength

   

InternalCouplerValue1

No

Yes

Yes

Not Required

MaxLength

   

InternalCouplerValue2

No

Yes

Yes

Not Required

MaxLength

   

InternalCouplerValue3

No

Yes

Yes

Not Required

MaxLength

   

IsInMdu

No

Yes

No

Not Required

None

   

IsLocked

No

Yes

Yes

Not Required

None

   

LastUser

No

Yes

Yes

Not Required

MaxLength

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

Manufacturer

No

No

No

Not Required

MaxLength

   

ModelNumber

No

No

Yes

Not Required

MaxLength

   

Name

No

No

Yes

Not Required

MaxLength

 

This field does not appear in the Attribute Editor, but is editable at the top of the device pane.

NetworkPath

No

Yes

No

Not Required

MaxLength

 

Can use FriendlyName="Network Path"

NodeId

No

Yes

No

Not Required

None

 

Can use FriendlyName="Node Id"

NodeLeg

No

Yes

No

Not Required

MaxLength

 

Can use FriendlyName="Node Leg"

NodeName

No

Yes

No

Not Required

MaxLength

 

Can use FriendlyName="Node Name"

OperationalForwardGain

No

No

No

Not Required

None

   

OperationalReturnGain

No

No

No

Not Required

None

   

PoweringFedFromComponentId

No

No

Yes

Not Required

None

   

PowerMode

No

Yes

No

Not Required

MaxLength

 

Can use FriendlyName="Power Mode"

PowerSupplyName

No

Yes

No

Not Required

MaxLength

 

Can use FriendlyName="Power Supply Name"

ReverseInputHighLevel

No

Yes

No

Not Required

None

 

Can use FriendlyName="Reverse Output High (dBmV)"

ReverseInputLowLevel

No

Yes

No

Not Required

None

 

Can use FriendlyName="Reverse Input High (dBmV)"

ReverseOutputHighLevel

No

Yes

No

Not Required

None

 

Can use FriendlyName="Reverse Output High (dBmV)"

ReverseOutputLowLevel

No

Yes

No

Not Required

None

 

Can use FriendlyName="Reverse Output Low (dBmV)"

SpecSymbology

No

Yes

No

Not Required

None

   

SymbolRotation

No

Yes

Yes

Not Required

None

 

Can use FriendlyName="Symbol Rotation"

UGStructureId

No

No

Yes

Not Required

None

   

Voltage

No

Yes

No

Not Required

None

   

Workflow_Status

Yes

Yes

Yes

CodedValueDomain

None

WorkflowState

Can use FriendlyName="Workflow Status"

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.