990–5809D-037

扭矩规格

螺栓规格

扭矩

M6

5 Nm (3.69 lb-ft)

M8

17.5 Nm (12.91 lb-ft)

M10

30 Nm (22 lb-ft)

M12

50 Nm (36.87 lb-ft)

反馈
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.