7EN02-0468-01

Configuration

The meter configuration can be performed through the HMI display or through communication tool via M-Bus or RS-485 Modbus.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?