7EN02-0468-01

Energy pulse output

RFT

SE

Action

Size

Type

Units

Description

Address

Register

Address

Register

0x1968

6505

0x1967

6504

R/WC

2

Float32

-

S0 output rate

Default: 1000

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?