7EN02-0468-01

Safety precautions

Installation, wiring, testing and service must be performed in accordance with all local and national electrical codes.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • This product must be installed inside a suitable fire and electrical enclosure.
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E in the USA, CSA Z462 or applicable local standards.
  • Do not install this product in hazardous or classified locations.
  • Product may use multiple voltage/power sources. Disconnect ALL sources before servicing.
  • Use a properly rated voltage sensing device to confirm that power is off.
  • Products rated only for basic insulation must be installed on insulated conductors.
  • Treat I/O wiring connected to multiple devices as hazardous live until determined otherwise.
  • Do not exceed the product’s ratings or maximum limits.
  • Replace the protection covers before powering the equipment.
  • Do not use this device for critical control or protection applications where human or equipment safety relies on the operation of the control circuit.
  • Do not use water or any liquid material to clean the product. Use a cleaning cloth to remove dirt. If dirt cannot be removed, contact local Technical Support representative.
Failure to follow these instructions will result in death or serious injury.
WARNING
RISK OF INJURY OR EQUIPMENT DAMAGE
  • Install the external fuse or thermal cut-off, external switch or single-pole circuit breaker on the phase line and not on the neutral line. The protection devices must be installed near to the meter.
  • The wire connecting the meter to the outside circuit, must be sized in accordance with local regulations for the maximum amount of the protection devices used in the circuit.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNING
Potential compromise of system availability, integrity, and confidentiality
  • Change the default password to help prevent unauthorized access to device configuration settings and information.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?