About this manual
Throughout the manual, the term “meter” / device” / “equipment” / “product” refers to iEM2435 / iEM2455 models. The differences between the models, such as a feature specific to one model, are indicated with the appropriate model number or description.
This manual assumes you have an understanding of single phase energy meters and are familiar with the equipment and power system in which your meter is installed.
This manual does not provide configuration information for advanced features where an expert user would perform advanced configuration. It also does not include instructions on how to incorporate meter data or perform meter configuration using energy management systems or software, other than Modbus and M-Bus tool.
Make sure you are using the most up-to-date version of your device’s firmware in order to access the latest features.
The most up-to-date documentation about your device is available for download from www.se.com.
Related documents
|
Document |
Number |
|---|---|
|
iEM2435 / iEM2455 instruction sheet |
JYT8368500 / JYT8368600 |