Communication
|
Command Number |
Action |
Size |
Type |
Unit |
Range |
Description |
|---|---|---|---|---|---|---|
|
5000 |
W |
1 |
UInt16 |
— |
— |
(Reserved) |
|
W |
1 |
UInt16 |
— |
— |
(Reserved) |
|
|
W |
1 |
UInt16 |
— |
— |
(Reserved) |
|
|
W |
1 |
UInt16 |
— |
1 – 247 |
Modbus ID |
|
|
W |
1 |
UInt16 |
— |
0 – 5 |
Baud Rate
|
|
|
W |
1 |
UInt16 |
— |
0 – 2 |
Parity
|
|
|
W |
1 |
UInt16 |
— |
— |
(Reserved) |
|
|
5100 |
W |
1 |
UInt16 |
— |
0 – 1 |
Register Map Selection
|