Program mode 3 (Pro-3) configuration
- Setting up pulse output rateThe meter is equipped with two pulse outputs (forward and reverse) which are optically isolated from the inside circuit. The meter generates pulses in proportion to the measured consumption for purpose of remote reading or accuracy testing. The pulse output is a polarity dependent, open-collector transistor output which requires an external voltage source for correct operation. For this external voltage source, the voltage (Ui) should be less than 27 V DC. The maximum switching current (Imax) is 100 mA. To connect the impulse output, connect 5 – 27 V DC to connector 18/20 (collector), and the signal wire (S) to connector 19/21 (emitter).
- Setting up combination codeThe meter allows you to display the total energy (usage) based on the combination code. The combination code is in accordance with different calculation methods as shown below:
- Setting up baud rateThe Modbus (iEM2455) baud rate can be set from 1200 to 38400. The M-bus (iEM2435) baud rate can be set from 300 to 9600.
- Setting the register mapThe register map is a structured table that defines how data is stored and accessed within the energy meter.
- Setting up parity (only iEM2455)The Modbus (iEM2455) parity can be set to EvEn, nonE or odd. The M-bus (iEM2435) parity is always EvEn.
- Resetting power down counterThe power down counter registers the number of times the meter has been turned off.
- Setting up passwordThe Program mode 3 (Pro-3) is protected with a password. The default password is 0000.
- Setting up OBIS codeYou can set the OBIS code to on in Program mode 3 (Pro-3). The default setting for OBIS code is oFF.
Parent topic: Configuring