7EN02-0468-01

Button functions

Action

Button function

Hold the up-arrow button or down-arrow button for less than 3 seconds

To enable scroll.

NOTE: After 30 seconds of no interaction the meter goes back to automatic scroll mode.

Hold the up-arrow button for 3 seconds

To enter the next menu.

Hold the down-arrow button for 3 seconds

To go back to previous menu.

Hold both down-arrow button and up-arrow button for 3 seconds

To confirm settings.

Hold the up-arrow button for ≥5 seconds

To enter program mode.

To add or remove from the automatic scroll.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?