7EN02-0468-01

Communication

RFT

SE

Action

Size

Type

Units

Description

Address

Register

Address

Register

0x1965

6502

0x1964

6501

R/WC

1

UInt16

-

RS-485 communication port address

1 – 247

Default: 1

0x1966

6503

0x1965

6502

R/WC

1

UInt16

-

RS-485 communication baud rate

  • 0 = 9600

  • 1 = 19200 (default)

  • 2 = 38400

  • 3 = 4800

  • 4 = 2400

  • 5 = 1200

0x1967

6504

0x1966

6503

R/WC

1

UInt16

-

RS-485 communication parity

  • 0 = Even (default)

  • 1 = Odd

  • 2 = None

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?