7EN02-0468-01

Setting the register map

The register map is a structured table that defines how data is stored and accessed within the energy meter.
NOTE: Select SE RMAP to access the register address that is one offset lower than the current RFT register address.
To set the register map:
  1. Press the up or down arrow button to navigate to Program mode 3 (Pro-3).
  2. Press and hold the up-arrow button for 3 seconds to open the menu.
  3. Press the up or down arrow button to choose each digit of the 4-digit password (default is 0000). Hold the up-arrow button for 3 seconds to confirm each digit.
  4. Press the up or down arrow button to scroll to the register map (RMAP) page.
  5. Press and hold the up-arrow button for 5 seconds to go to program mode.
  6. Press the up or down arrow button to select rFt / SE when the value starts blinking.
  7. Press and hold both buttons for 3 seconds to confirm the new setting.
Result: The meter displays “OK” on the LCD to confirm the setting.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?