7EN02-0468-01

Viewing instantaneous (RMS) measurements

  1. Scroll with the buttons to active power (REAL) register in the main menu.
  2. Hold the up-arrow button for 3 seconds to enter the next menu.
    The display shows >>.
  3. Hold the down-arrow or up-arrow button to scroll through various instantaneous (RMS) measurement pages.
  4. Hold the down-arrow button for 3 seconds to go back to main menu.
    The display shows <<.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?